2018-08-13 11:29 PM
I want to get gps information using p nucleo lrwan1. Can I get an open source that can help? I'll use the uart port.(gps)
2018-08-14 5:49 AM
Hello,
I am afraid this is not possible. LoRa operates in EU at 868 MHz and 915 MHz in the US. However, GPS utilizes 1575.42 MHz (10.23 MHz × 154) called L1 and 1227.60 MHz (10.23 MHz × 120), called L2.
David
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.