2016-09-12 12:05 AM
I am using HTS221 for humidity and temperature measurement.
On reading the registers for temperature and converting as per the equation suggested, i get the correct temperature. but on reading the registers for humidity and converting as per the equation suggested, humidity obtained is not correct. the register values read are as follows: H0_T0_OUT = 9 H1_T0_OUT = -10540 H0_RH_X2 = 53 H1_RH_X2 = 132 when humidity is measured in a controlled environment with different known humidities, the HTS221 measured humidity varies +/- 5 % within the range 26.5 % to 66% humidity(which is calibrated range of sensor), but outside the range that is lower than 26.5% and higher than 66% variation of 10 to 20% humidity is seen. kindly help to get the correct humidity. regards unnati2016-11-03 11:17 AM
HTS221 AV_CONFIG: 0x10 value is 0x3F
HTS221 CTRL_REG1: 0x20 value is 0x83
HTS221 CTRL_REG2: 0x21 value is 0x00
HTS221 CTRL_REG3: 0x22 value is 0x00
In Humidity registers I get the following values listed below:
H_T_out(s16) = -9349 - > two complements:
9349
H0_rH(s16) = 27
H1_rH(s16) = 66
H0_T0_OUT(s16) = 0
H1_T0_OUT(s16) = -10442
- > two complements:
10442
With this values I applied the following formula :tmp = ((uint32_t)(H_T_OUT - H0_T0_OUT))*((uint32_t)(H1_rH - H0_rH)*10);humidity = tmp/(H1_T0_OUT - H0_T0_OUT);humidity += H0_rH*10;Using the signal the final value is:humidity = -619 -> 61,9%
Someone could help me to get the correct humidity readings?Regards2017-05-06 3:24 PM
Hello, please have a look at my post here:
https://community.st.com/0D50X00009XkXwhSAF
I use a different casting and get the correct result.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.