2019-07-26 9:01 AM
I am using the MEMSMIC1 Microphones_Streaming example (https://www.st.com/en/embedded-software/x-cube-memsmic1.html) with the STM32WBxx chip.
I am trying to change the clocking pin from PB13 to PB8 to use the example with custom hardware.
I am trying to do this by modifying the pin definitions in the ccm02m1_audio.h file:
#ifdef USE_STM32WBXX_NUCLEO /* defines valid only for STM32WB */
/* I2S Configuration defines */
#define AUDIO_IN_SAI_INSTANCE SAI1_Block_A
#define AUDIO_IN_SAI_CLK_ENABLE() __SAI1_CLK_ENABLE()
#define AUDIO_IN_SAI_SCK_PIN GPIO_PIN_8
#define AUDIO_IN_SAI_SCK_GPIO_PORT GPIOB
#define AUDIO_IN_SAI_SCK_GPIO_CLK_ENABLE() __GPIOB_CLK_ENABLE()
#define AUDIO_IN_SAI_SCK_AF GPIO_AF13_SAI1
#define AUDIO_IN_SAI_SD_PIN GPIO_PIN_15
#define AUDIO_IN_SAI_SD_GPIO_PORT GPIOB
#define AUDIO_IN_SAI_SD_GPIO_CLK_ENABLE() __GPIOB_CLK_ENABLE();
#define AUDIO_IN_SAI_SD_AF GPIO_AF13_SAI1
I am able to change change to PA8 but not PB8.
PB8 uses MCLK rather than SCK and so I believe this might be the issue.
Does anyone know how I might get around this problem?
Finlay
2019-07-30 1:55 AM
Hi @FFlet , consider that the SAI samples on the bit clock, and not on the master clock, and on PB8 the MCLK is running. However, you could set the SAI interface in a proper way, making the bit clock same as master clock, e.g. in these two ways:
Regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.