2023-11-07 5:55 AM
In my design, when setting the ODR = 100Hz or below , I can get 100hz INT signals , and received 100 sets vibration data every Second. (Using XYZ data-ready as int1)and modify the ODR setting to 200Hz , just get 200 hz INT signals ,and received 145 sets data。
How to improve the actual ODR ? We want realize 1.376KHz @hr mode
or 5.376kHz @LP mode, Which mcu is suitable ? STM32F103 70MHz ? or higher End ?
And I2C interface is suitable for 5.376kHz ? or must be SPI ?
2023-11-09 11:29 PM
Hi @JohnGe ,
You need to use SPI @ 10MHz and an powerful mcu to manage that interrupt velocity such as a STM32U5.
For further questions I suggest you to open a topic on the MCU forum.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.