2020-05-22 12:55 AM
Hi, I am reading the datasheet of LSM9DS1 and it says that there are two times (rise and wait) you should respect
I was thinking in a sequencer IC but if we see the schematic of the LSM9DS1 evaluation board (STEVAL-MKI159V1) it does not use any kind of external IC to control the power up time, they just connects the Vdd and Vdd_IO directly to the power supply, why?, is there no consequence in supply the IMU without meet the requirements of the datasheet?, thanks
2020-05-22 4:49 AM
Hi @jg_spitfire , considering the schematic of the STEVAL-MKI159V1 you posted above, there is no short path between Vdd and Vdd_IO: the two lines are separated and are supposed to be tied to a couple of application processor (uC) pins: this is coherent with the sequential power-on scheme of the datasheet. What I however can tell you is that 99.9% of the times you will not encounter issues in connecting together the Vdd and the Vdd_IO lines (but in this way you will maybe have a little extra current consumption in power down), provided that your Vdd / Vdd_IO ramp is not too fast (<< Trise). Regards
2020-06-02 10:34 AM
Hi, so I understand that I should implement the delay between the two pins, I am thinking in use a soft start LDO for each pin because with the uC I can not control the Vdd_IO rise time, what do you think?, is there any datasheet with that circuit reference? , thanks
2020-06-02 10:52 AM
datasheet, page 14:
For the power-up sequence please refer to the following figure, where:
• Trise is the time for the power supply to rise from 10% to 90% of its final value
• Twait is the delay between the end of the Vdd_IO ramp (90% of its final value) and the
start of the Vdd ramp
why does the start up requirements are so restrictive?, I need to provide a controlled Trise and in the precise time when Vdd_IO achieves the 90% of its final value then start counting the Twait, right?
2021-10-20 9:34 AM
Hi,
I followed the discussion and I'm wondering if at the end you figured out how to power up correctly the MKI159V1 module.
Thanks in any case.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.