2021-09-29 4:33 AM
We are using LSM6DSOXTR Sensor for getting the acceleration,
Its datasheet says
(4.6.2- Zero-g and zero-rate level Page no 17)"A sensor in a steady state on a horizontal surface will measure 0 g on both the X-axis and Y-axis, whereas the Z-axis will measure 1 g."
but we are getting below values,
X Y Z
13 65531 64541
13 65532 64542
6 65530 64539
8 65531 64540
Can anyone suggest
1)Why we are getting this much high values?
2)How to achieve the value "0" in the X, Y-axis when the sensor is put on a flat non-moving surface?
It will be more helpful if someone shares a sample code which is showing the settings and process to get correct acceleration data.
Thanks
Solved! Go to Solution.
2021-09-30 1:32 AM
Hi @Shivam Paliwal ,
please note that the data you are getting has to be converted from LSB to physical units (in this case, milli-g) through two's complement conversion.
You can find example of these conversion formulas in C on Github driver page --> lsm6dsox_reg.c
Supposing you have configured your device in Normal mode, and with a +-2g FullScale (is this assumption correct?), you have:
float_t lsm6dsox_from_fs2_to_mg(int16_t lsb)
{
return ((float_t)lsb) * 0.061f;
}Data output:
X axis --> 13 LSB = 13 DEC = 0.8 mg [correct]
Y axis --> 65531 LSB = -5 DEC = -0.3 mg [correct]
Z axis --> 64541 LSB = -955 DEC = -60.7 mg [this is low, should be around 1000 mg. Are you applying some filters?]
If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster
-Eleon
2021-09-30 1:32 AM
Hi @Shivam Paliwal ,
please note that the data you are getting has to be converted from LSB to physical units (in this case, milli-g) through two's complement conversion.
You can find example of these conversion formulas in C on Github driver page --> lsm6dsox_reg.c
Supposing you have configured your device in Normal mode, and with a +-2g FullScale (is this assumption correct?), you have:
float_t lsm6dsox_from_fs2_to_mg(int16_t lsb)
{
return ((float_t)lsb) * 0.061f;
}Data output:
X axis --> 13 LSB = 13 DEC = 0.8 mg [correct]
Y axis --> 65531 LSB = -5 DEC = -0.3 mg [correct]
Z axis --> 64541 LSB = -955 DEC = -60.7 mg [this is low, should be around 1000 mg. Are you applying some filters?]
If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster
-Eleon
2021-10-06 5:39 AM
Hi @Shivam Paliwal ,
do you have any news about this issue?
-Eleon
2021-10-07 1:26 AM
Hi @Eleon BORLINI ,
Thank You so much for your response ...
and apologies for the delayed reply..
Your reply helped us a lot.
Below is the raw data that we got from the sensor (Physical condition of PCB- Accelerometer PCB is not moving and put flat on the plastic table)
8bit 8bit 8bit 8bit 8bit 8bit
X-low X-high Y-low Y-high Z-low Z-high
29 0 34 1 76 192
223 0 35 1 177 192
54 1 175 0 41 193
6 1 99 0 116 192
143 0 141 0 103 193
35 1 155 0 227 186
204 255 27 2 250 191
126 0 18 1 87 194
167 0 12 1 44 192same data in combined 16 bit
16bit 16bit 16bit
X-combined Y-combined Z-combined
29 290 -16308
223 291 -16207
310 175 -16087
262 99 -16268
143 141 -16025
291 155 -17693
-52 539 -16390
126 274 -15785
167 268 -16340
and after multiplying it with Sensitivity +-2g (i.e 0.061)
We got the below values..
X in mg Y in mg Z in mg
1 17 -994
13 17 -988
18 10 -981
15 6 -992
8 8 -977
17 9 -1079
-3 32 -999
7 16 -962
10 16 -996I am assuming it is in mg..
Can you please tell
1)Is my understanding correct for the conversion process and unit of X Y Z??
2)When we convert this data in mm/sec2 (1 g = 9806.65 mm/s2.), We get the below values
X in mm/s2 Y in mm/s2 Z in mm/s2
9.80665 166.71305 -9747.8101
127.48645 166.71305 -9688.9702
176.5197 98.0665 -9620.32365
147.09975 58.8399 -9728.1968
78.4532 78.4532 -9581.09705
166.71305 88.25985 -10581.37535
-29.41995 313.8128 -9796.84335
68.64655 156.9064 -9433.9973
98.0665 156.9064 -9767.4234Do you think these values are correct even if Accelerometer PCB is just lying on the plastic table??
Used below function from lsm6dsox_reg.c for getting raw acceleration data from the sensor.
/**
* @brief Linear acceleration output register.
* The value is expressed as a 16-bit word in two’s complement.[get]
*
* @param ctx read / write interface definitions
* @param buff buffer that stores data read
*
*/
int32_t lsm6dsox_acceleration_raw_get(stmdev_ctx_t *ctx, uint8_t *buff)
{
int32_t ret;
ret = lsm6dsox_read_reg(ctx, LSM6DSOX_OUTX_L_A, buff, 6);
return ret;
}Sorry for such a big question...
Thanks.
2021-10-07 3:59 AM
Hi @Shivam Paliwal ,
1) Is my understanding correct for the conversion process and unit of X Y Z??
Right, the values look correct (along Z you see the 1g gravity acceleration) and
2) Do you think these values are correct even if Accelerometer PCB is just lying on the plastic table??
The conversion from mg into mm/s2 is correct. Consider that there can be a residual Zero g level (±20mg, see datasheet, p.10).
If you want to reduce this value, you can characterize it in a steady state and then write the value into the X_OFS_USR (73h), Y_OFS_USR (74h) and Z_OFS_USR (75h) registers, enabling the USR_OFF_ ON_ OUT bit of 1 CTRL7_G (16h) register.
The function you reported is ok.
If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster
-Eleon
2021-10-08 12:28 AM
Hi @Eleon BORLINI
Thanks for the data validation...
We will try residual Zero-g level settings and let you know the result...
Regards,
Shivam
2021-12-23 7:13 AM
Hi @Eleon BORLINI
as you know ,
We are using LSM6DSOXTR Sensor for getting the acceleration
Accelerator data coming from ST Sensors showing very high value of acceleration,
when compared to other Product such as XYZ brand.
We mounted ST Sensor on an Industrial equipment, we get Acceleration data in mm/sec2 as below.
(We converted from mg to mm2 by ((value in mg/1000)*9806.65) )
Y(in mm/sec2) X(in mm/sec2) Z(in mm/sec2)
8904.4382 4462.02575 5913.40995
9649.7436 5040.6181 3196.9679
10042.0096 2098.6231 696.27215
10865.7682 -961.0517 4177.6329
10669.6352 -6040.8964 3206.77455
10238.1426 -3991.30655 4001.1132
9306.51085 -1078.7315 1490.6108
9590.9037 2000.5566 98.0665
8227.77935 176.5197 -1990.74995
8727.9185 -2441.85585 3628.4605When we mount Sensor from other brand XYZ, and measured vibration for same condition, we get below values.
x(in mm/sec2) y(in mm/sec2) z(in mm/sec2)
9.439 7.57 1.122
8.785 6.168 5.327
6.823 2.056 5.047
8.411 1.963 3.084
9.907 6.262 6.262
7.29 3.178 9.253
5.327 2.71 11.776
6.823 1.963 20.374
5.421 1.589 24.113
0.467 0.935 22.43There is huge difference between these values coming from 2 sensors for exactly same conditions.
We then calculated VRMS from acceleration data from ST Sensor and XYZ sensor. With ST sensor it is coming abnormally high data.
Effectively we understand acceleration data coming from ST sensor is high value than it should be, but we are not sure, reason for this.
When we just keep ST sensor on stationary surface, we get acceleration data in mm/sec2 as below. (converted from mg)
X in mm/s2 Y in mm/s2 Z in mm/s2
9.80665 166.71305 -9747.8101
127.48645 166.71305 -9688.9702
176.5197 98.0665 -9620.32365
147.09975 58.8399 -9728.1968
78.4532 78.4532 -9581.09705
166.71305 88.25985 -10581.37535
-29.41995 313.8128 -9796.84335
68.64655 156.9064 -9433.9973
98.0665 156.9064 -9767.4234This looks to be very large. Can you please throw some light??
Regards,
Shivam
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.