cancel
Showing results for 
Search instead for 
Did you mean: 

How do I send data from Algobuilder to an app vía bluetooth with Sensortile.box??

LRoss.1
Associate

Hi everyone,

I need to send data I get from Algobuilder app to and app I've made with appInventor. I want to send it via bluetooth​ and I'm using the sensortile.box. How can I do It??

Thanks!​

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Eleon BORLINI
ST Employee

Hi @LRoss.1​ , in the latest version 2.5 of AlgoBuilder there is the firmware template for SensorTile.box with BLE communication. Please note that this communication works with Unicleo-GUI. Theoretically it is possible to use the firmware for communication with any other application but the protocol is proprietary, so the only way it to reverse engineer the protocol from the firmware source code. You ask more information to the STMicroelectronics sales office and representatives of your geographical area. Regards

DWind.1
Associate III

Hi! I am currently trying the same. Everything is ok if I select "SensorTile.box" as the target, Unicleo shows the data transferred via COM port. If I chose "SensorTile.box BLE" a Bluetooth device with the name "ALGOB" appears. The problem is, that I cannot connect my PC or my mobile phone to this device. Windows shows the PIN, but if confirm this pin, it fails to connect. Same with the mobile phone. Any hint what could be the problem?

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.