2022-04-28 8:51 AM
Hi,
I wanted to replace the SD card of the sensortile.box with a faster one, but then I am not able to upload my application. Does anyone know what the problem could be?
Thanks in advance and best regards, Carla
2022-04-29 8:41 AM
Hi Carla @CTett.1 ,
there should not be any problem with faster sd cards
I don't think that the datalog speed depends on the sd card speed, so I don't recommend to change it.
anyway, if you want to use that one, try to format it before using it, maybe the firmware is not able to write the flow on the card.
please, check if there is a DefaultApp.json file in it.
Niccolò
2022-05-02 12:27 AM
Hi Niccolò @niccolo.ruffini ,
Thanks for the answer, unfortunately formatting the SD card before using it doesn't help. There is no DefaultApp.json file after setting the firmware. What else could be the problem?
Thanks for your help and best regards,
Carla
2022-05-02 2:01 AM
Hi Carla @CTett.1 ,
let me try to ask you a few question to understand
1- are you able to read/write the sdcard without using the sensortile.box?
2- what class and size is the sdcard?
3- if you upload a new application I imagine that you get an error, but what if you connect to the board? is there the new application running, or the previous one?
Niccolò
2022-05-03 7:38 AM
Hi Niccolò @niccolo.ruffini ,
Thank you a lot for your help,
Carla
2022-05-04 1:59 AM
Ciao Carla @CTett.1 ,
there's something strange in the flow,
but first, can you post the defaultApp.json file that you are using, so I can confirm the right behaviour for the flow you are uploading?
Niccolò
2022-05-04 5:57 AM
Hi Niccolò @niccolo.ruffini ,
Yes sure, You can find it in the attachment, I just converted it to .txt that I am able to upload it. But I actually tried it again with copy paste from the normal SD card and using it like that, but know the new SD card is empty after the recording.
Thank you very much for your help, Best Carla
2022-05-27 7:41 AM
Hi Carla,
sorry for the delay in the answer, the json file is not what I'd expect, I fear that an sdcard of that type is not supported
can I ask you why do you think the problem in writing speed is due to the sdcard?
Niccolò
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.