2021-06-26 8:29 PM
Hi guys,
Now I have some troubles with 2 VL53L1X that measure the distance at the same time but I can't init these sensor ? Here my code I code on Esp32. I'm using SparkFun library
https://github.com/sparkfun/SparkFun_VL53L1X_Arduino_Library.git
#include <Arduino.h>
#include <WiFi.h>
#include <Wire.h>
#include <Ethernet.h>
#include <SPI.h>
#include <VL53L1X.h>
#define SHUTDOWN_PIN 2
#define INTERRUPT_PIN 3
#define Sensor1_newAddress 47
#define Sensor2_newAddress 45
SFEVL53L1X Sensor1;
SFEVL53L1X Sensor2;
uint16_t distance0, distance1;
// #define SHUTDOWN_PIN 2 // có thể mở
// #define INTERRUPT_PIN 3
#define XSHUT_pin1 33
#define XSHUT_pin2 32
void setup (void)
{
Wire.begin();
Wire.setClock(400000); // use 400 kHz I2C
Serial.begin(115200);
Serial.println("Begin.....");
Wire.begin();
Wire.setClock(300000);
pinMode(XSHUT_pin1, OUTPUT);
pinMode(XSHUT_pin2, OUTPUT);
pinMode(XSHUT_pin1, INPUT);
if (!Sensor1.init())
{
Serial.println("VL53L1X custom sensor, Failed to detect and initialize sensor1!");
while (1);
}
delay(10);
Sensor1.setI2CAddress(Sensor1_newAddress);
pinMode(XSHUT_pin2, INPUT);
if (!Sensor2.init())
{
Serial.println("VL53L1X custom sensor, Failed to detect and initialize sensor2!");
while (1);
}
delay(10);
Sensor2.setI2CAddress(Sensor2_newAddress);
// Sensor1.setTimeout(500); // có thể mở
// Sensor2.setTimeout(500);
Sensor1.setDistanceModeLong();
Sensor1.setTimingBudgetInMs(50000);
Sensor2.setDistanceModeLong();
Sensor2.setTimingBudgetInMs(50000);
}
void loop(void)
{
distance0 = Sensor1.getDistance(); // return distance
Sensor1.stopRanging(); //Stops taking measurements // after measure the first distance stop measurement
Sensor1.clearInterrupt(); // Clear the interrupt flag // clear the interrupt
distance1 = Sensor2.getDistance(); // return distance
Sensor2.stopRanging(); //Stops taking measurements // after measure the first distance stop measurement
Sensor2.clearInterrupt(); // Clear the interrupt flag // clear the interrupt
Serial.print("Distance 0: ");
Serial.println(distance0);
Serial.print("Distance 1: ");
Serial.println(distance1);
return;
}
Thanks for help
2021-06-28 7:23 AM
I didn't read all the code, but I have 2 suggestions.
1 - your MCU is much faster than the sensors, I think you will find a 'wait_for_booted' in that library somewhere.
You were turning the sensor on in one clock cycle and initializing it in the next. It's a good sensor, but it does have to boot up.
(or you can just wait a few milliseconds.)
2 - The other trick is that the I2C is generally specified by the write address - and those have zero's in the LSbit.
It's also a superstition of mine that I put more distance between the addresses. You are right that they have to be 2 apart, but I've had better luck with 10 appart.
Download
2D LIDAR using multiple VL53L1X Time-of-Flight long distance ranging sensors.
It has an example of how we did 9 sensors. It will give you some ideas.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.