cancel
Showing results for 
Search instead for 
Did you mean: 

HDPE triggering Tpresence for STHS34PF80

Megatronic
Associate

We are designing an STHS34PF80 into an occupancy sensor and the plan is to have an HDPE window to protect it.  To test the response in the actual product we purchased 1/16" (1.5mm) HDPE sheet and put it over the sensor.  The fresnel lens with the dev kit was removed.  Surprisingly the Tpresence triggers when the sheet is over the sensor, and so the device doesn't seem to be seeing through the HDPE sheet.

My first thought is that the HDPE is doped or just wrong somehow but I thought I'd ask if anybody else has seen something like this.

Thank you.

1 ACCEPTED SOLUTION

Accepted Solutions
Federica Bossi
ST Employee

Hi @Megatronic ,

 

When you put the lens in front of the sensor, you are changing the working condition of the system, therefore it's necessary to perform a reset of the algorithm. You can follow the procedure in the AN5867 paragraph 7.4.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Federica Bossi
ST Employee

Hi @Megatronic ,

 

When you put the lens in front of the sensor, you are changing the working condition of the system, therefore it's necessary to perform a reset of the algorithm. You can follow the procedure in the AN5867 paragraph 7.4.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Thank you.  That worked.

 

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.