2017-09-14 5:24 AM
I have recently bought a STM32 Dev board with a X-NUCLEO_IKS012A mems sensor. I am new to embedded software and decided to get one of the example projects going for this board. I have gone through all the readme's etc. but st doesn't specify where to save the example project when downloaded from the internet. I get the following error:
make: *** No rule to make target `C:/Users/Charl Smalberger/Src/com.c', needed by `Example/User/com.o'. Stop.
Looks like a path related error.
I am using system workbench. I have attached the readme with basic instructions that i followed, the workbench instructions are at the bottom.
Please can anyone assist?
#isk01a22017-09-14 7:59 AM
I suppose you have downloaded the X-CUBE-MEMS1 package from st.com.
You can extract it, for example to your C:\ drive.
Then execute the SW4STM32 and set the workspace path to the project you want to try, for example:
C:\STM32CubeExpansion_MEMS1_V4.0.0\Projects\Multi\Examples\IKS01A2\LSM6DSL_FIFOLowPower\SW4STM32\STM32L152RE-Nucleo
Then import the project: File -> Import, Select General -> Existing Project into Workspace then click Next
Click Browse on Select root directory, the right directory is selected so you click, OK then Finish.
After that you have the project in your workspace and you can Build it.
2017-09-15 7:33 AM
Thank You Miroslav it worked!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.