2023-10-17 12:31 AM - last edited on 2023-10-18 6:33 AM by Imen.D
Hi,
I'm Working with H3LIS331DL Accelerometer and STM32F410 for vibration test(Levels:0.04 g^2/Hz,2O Hz to 2000 Hz All 3 Axis, 5 Minutes each axis) at SPI mode.I have readed the raw data from the H3LIS331DL and communicated it by UART. But after that,I have no idea how to use my raw data for my project requirement,can someone help me with this.About,How the raw Data conversion has been done and about the different output units of Accelerometer(for example-g,mg/digit.m/s^2). Thanks in advance.
2023-10-17 6:04 AM
1 g = 9.8 m/s^2
1 mg = 0.001 g
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.