cancel
Showing results for 
Search instead for 
Did you mean: 

For X-NUCLEO-IKSO1A3 and NUCLEO-L476RG only options IKSO1A1 and IKSO1A2 which are working well but not option IKSO1A3 with STM32CubeExpansion_MEMS1_V4.4.1

PWeil.2
Associate

in order to get all sensor working

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Imen.D
ST Employee

Hello @PWeil.2​,

You are right, the X-CUBE-MEMS1 expansion package version 4.4.1 supported the STM32L476RG devices and NUCLEO-L476RG board with X-NUCLEO-IKS01A1 and X-NUCLEO-IKS01A2 Boards.

You can check this history and main changes in the "Release notes" file of the package.

Note that the NUCLEO-L476RG examples and applications are replaced by NUCLEO-U575ZI-Q ones, since the release V9.3.0 of X-CUBE-MEMS1 expansion package.

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.