cancel
Showing results for 
Search instead for 
Did you mean: 

Does ST offer any IP67 microphones with analog output?

LCE
Principal II

Does ST offer any IP67 microphones with analog output?

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Federica Bossi
ST Employee

Hi @LCE ,

All MEMS microphones have a hole through which water surely enters and therefore there are no water-resistant MEMS microphones on the market

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
LCE
Principal II

But as you surely have experienced, sound waves can travel through solid matter. ;)

Infineon IM73A135V01 (but that one has a differential output, I'd rather have it single-ended, but that's not specified for that mic) has at least IP57:

IP5x: Ingress of dust is not entirely prevented, but it must not enter in sufficient quantity to interfere with the safe operation of the equipment.

IPx7: Immersion, up to 1 meter (3 ft 3 in) depth Ingress of water in harmful quantity shall not be possible when the enclosure is immersed in water under defined conditions of pressure and time (up to 1 meter (3 ft 3 in) of submersion). Test duration: 30 minutes

Until recently we used a microphone from Vesper (also IP57), but that small company was bought and that product EOL'd.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.