2018-10-31 8:10 PM
Hi,
from Data sheet, i saw section 3.5, it says no need to further calibration
but when i check output data from register 28-2D, the value is variety time to time ,
it has variety range for +- 20 ~ +-40, is it correct? or we should do calibration at factory side?
regards
Gary
2018-11-01 1:25 AM
What is the unit of mentioned variance? mg? LSB?
In any case some variance is normal, the sensor has a noise, a noise can be also induced by not completely stable environment.
Additional calibration is not needed.
2018-11-01 2:15 AM
Hi
thanks for reply, i guess the unit should be mg
output_x = (value from register 28-29) * sensitivity
the sensitivity is define as "#define SENSITIVITY_2G 1 /** mg/LSB */"
i also do some calculate with sqrt(output_x^2 + output_y^2 + output_z^2)
the variance is still.
am i go wrong with definition or something else?
regards
Gary
2018-11-01 6:24 AM
The sensor has several modes and according to the mode the output is 8, 10 or 12 bit left adjusted in the output 16 bit register. So you have to shift right the value in output register.
You can check your conversion is correct if you see 1g of the gravity in an axis pointing to ground.
2018-11-01 6:36 PM
Hi,
my setting is 10 bit with normal mode, with FS = +-2g, ODR = 100Hz
and i've measure for 5 minutes with 5 times, the average of conversion is 1010 mg, point to ground
regards
Gary
2018-11-02 2:28 AM
OK, it looks good.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.