2021-03-03 8:20 AM
Solved! Go to Solution.
2021-03-03 9:28 AM
there are many examples, you can refer to Github repository highlighted in webinar material for some. In particular, in the context of the IIS2ICLX, the mentioned application for monitoring the traffic load on a bridge rely on combined usage of FSM and MLC
The other example showed in the webinar is the direct angle output from inclinometer based on MLC classification. With other ST sensors with MLC, we have also examples of detecting if drilling machine is idle, tightening screw or drilling to wood etc, this type of example could then be extended to automated machinery and this example can be for sure adapted also to run on IIS2ICLX.
2021-03-03 9:28 AM
there are many examples, you can refer to Github repository highlighted in webinar material for some. In particular, in the context of the IIS2ICLX, the mentioned application for monitoring the traffic load on a bridge rely on combined usage of FSM and MLC
The other example showed in the webinar is the direct angle output from inclinometer based on MLC classification. With other ST sensors with MLC, we have also examples of detecting if drilling machine is idle, tightening screw or drilling to wood etc, this type of example could then be extended to automated machinery and this example can be for sure adapted also to run on IIS2ICLX.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.