2013-09-17 6:53 AM
Hello!
I have a question about the LSM303DLHC. In the data sheet i can't found any information about the output format for the acceleration and magnetic data. Therefore i thought it works with 16-bit values. While using the sensor I noticed that the acceleration data I get are wrong. After some search in the web and some test I recognized that the acceleration data are 12-bit left-justified and the magnetic data are 12-bit right-justified. The information I found on: Now I hope anyone can confirm my experience?!Greetings Oliver Lubritz #accelerometer #lsm303dlhc-data-format #data2013-09-18 8:53 AM
Hello Oliver,
Yes, your experience is correct, the magnetometer data is right-justified and the accelerometer data is left�justified, in normal mode, the data is in 12�bit representation which means the lowest 4 bit in LSB are always 0s. In low power mode, the data is in 8�bit representation which means only MSB has real dataand LSB is always 00h.
I hope this clarifies your question, and please feel free to post any other topics that you would like to discuss. Thank you, Thiago ReisWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.