2024-05-15 5:47 AM - edited 2024-05-15 11:56 AM
In the project I use Attiny13a) +
LIS2DH SPI interface.
One leg of the microcontroller is
missing.
Is it possible in SPI mode to
connect the CS pin directly to GND,
and not to the microcontroller port.
In I2C mode there are enough pins,
everything works fine, but the
current consumption is too high.
2024-05-16 5:08 AM
Hi @Artem777 ,
What current consumption do you get that is too high?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.