cancel
Showing results for 
Search instead for 
Did you mean: 

Connect WBA55CG + LIS2DUX12

Henry_BLE
Associate II

Hello everyone,

 

I'm new to both BLE and MEMS sensor. I want to combine 2 examples code as following:

STMems_Standard_C_drivers/lis2dux12_STdC/examples/lis2dux12_mlc_activity_mobile.c at master · STMicroelectronics/STMems_Standard_C_drivers · GitHub

 

STM32WBA Bluetooth® LE – Serial communication - stm32mcu

 

so that i can send MEMS events via BLE/USART. Could someone give me support or instruction, how to combine ?

1 ACCEPTED SOLUTION

Accepted Solutions
Federica Bossi
ST Employee

Hi @Henry_BLE ,

Hello,

Regarding the use of the STM32WBA microcontroller and BLE (Bluetooth Low Energy) technology, I would like to provide you with some advice and operational guidelines to facilitate the development of your application.

Useful Resources

On the official STMicroelectronics wiki, you can find numerous practical examples demonstrating how to use the STM32WBA microcontroller with BLE. In particular, I suggest consulting the following example:
STM32WBA Heart Rate Example
This example is especially useful as it presents a complete application for BLE data transmission and reception via a mobile app, covering both firmware implementation and communication management.

Recommended Development Approach

To optimize the development process, I suggest proceeding gradually by following these steps:

  1. Implement UART serial communication without BLE
    Start by creating a basic firmware that manages UART serial communication. This will allow you to verify and test data transmission simply and reliably, without introducing the complexity of the BLE protocol.
  2. Study and integrate the WPAN system for BLE
    Next, deepen your understanding of the WPAN  system used to manage BLE communication. You can rely on example firmware and documentation available on the ST wiki to understand how to configure and handle BLE communication on the STM32WBA microcontroller.
  3. Integrate UART and BLE communication
    Once you are familiar with both systems, you can integrate UART and BLE communication within the firmware. Essentially, during data transmission via WPAN, it will be possible to also send data over UART, enabling dual communication modes and facilitating debugging and monitoring.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Federica Bossi
ST Employee

Hi @Henry_BLE ,

Hello,

Regarding the use of the STM32WBA microcontroller and BLE (Bluetooth Low Energy) technology, I would like to provide you with some advice and operational guidelines to facilitate the development of your application.

Useful Resources

On the official STMicroelectronics wiki, you can find numerous practical examples demonstrating how to use the STM32WBA microcontroller with BLE. In particular, I suggest consulting the following example:
STM32WBA Heart Rate Example
This example is especially useful as it presents a complete application for BLE data transmission and reception via a mobile app, covering both firmware implementation and communication management.

Recommended Development Approach

To optimize the development process, I suggest proceeding gradually by following these steps:

  1. Implement UART serial communication without BLE
    Start by creating a basic firmware that manages UART serial communication. This will allow you to verify and test data transmission simply and reliably, without introducing the complexity of the BLE protocol.
  2. Study and integrate the WPAN system for BLE
    Next, deepen your understanding of the WPAN  system used to manage BLE communication. You can rely on example firmware and documentation available on the ST wiki to understand how to configure and handle BLE communication on the STM32WBA microcontroller.
  3. Integrate UART and BLE communication
    Once you are familiar with both systems, you can integrate UART and BLE communication within the firmware. Essentially, during data transmission via WPAN, it will be possible to also send data over UART, enabling dual communication modes and facilitating debugging and monitoring.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.