cancel
Showing results for 
Search instead for 
Did you mean: 

Compatibility of the IMP23ABSUTR Sensor with Vapor Phase Reflow Ovens

Moe_Rice
Associate II

Hello,

Can the IMP23ABSUTR sensor go through a vapor phase oven?"

Thx.

 

 

1 ACCEPTED SOLUTION

Accepted Solutions

Hi @Moe_Rice ,

it is not recommended to solder microphones with that technique, because they have a hole through which contamination enters. I suggest you use IR reflow ovens.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

6 REPLIES 6
Andrew Neil
Super User

Did you look at the "Soldering Information" section in the datasheet?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
Moe_Rice
Associate II

Hello,

The datasheet does not specifically mention vapor phase soldering. It generally refers to the compatibility of the IMP23ABSUTR sensor with the reflow soldering process and provides a recommended thermal profile for lead-free (Pb-free) soldering.

The term "vapor phase" is not explicitly mentioned in the documentation, and the information provided mainly concerns temperature parameters, preheat time, duration above the melting temperature, and peak temperature. In my opinion, these guidelines could potentially be adapted to different types of reflow processes, including vapor phase soldering, but this would require specific validation.

Thx

Hi @Moe_Rice ,

it is not recommended to solder microphones with that technique, because they have a hole through which contamination enters. I suggest you use IR reflow ovens.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Sounds like that should be explicitly explained in the datasheet?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

I will notice to the team!

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
acrova
Associate

I have notice IMP23ABSUTR NRND.  

Did thst mens it will be face out.  If yes.  Is there any replacement  upcomming for 80khz ultrasonic  mems microphone? 

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.