cancel
Showing results for 
Search instead for 
Did you mean: 

Can i use STEVAL-MKI208V1K standalone ?

bcryhun
Associate II

I have STEVAL-MKI208V1K but not its own compatible motherboard. I want to use IIS3DWB sensor. When i connec SDA, SCL, GND and VDD(for vdd i have tried 3v3 and 5v), HAL_OK said HAL_ERROR. Is this STEVAL-MKI208V1K can be used standalone or no?

Thanks for helping

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Peter BENSCH
ST Employee

The STEVAL-MKI208V1K is just an adapter board with a sensor that makes the pins accessible via connectors. Of course, you can also use it stand-alone. However, the included IIS3DWB will almost certainly be destroyed by 5V supply voltage. When trying again, please do not forget the pull-ups on the I2C lines.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.