2021-04-28 5:36 AM
Hello,
I can not find any information on calibration of the acetometer in the LIS2DW12.
Is it something we can do ourselves, is it done automatically etc.
Would like a reference or explanation.
Thank you
Solved! Go to Solution.
2021-04-28 6:50 AM
Hi @Msaga.1 ,
the accelerometer is calibrated at production level, and the calibration values are stored in the reserved registers, and it is better to not modify them.
However, it could happen that after the soldering process or handling actions, the accelerometer might be slightly out of calibration, and in this case you can:
If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster.
-Eleon
2021-04-28 6:50 AM
Hi @Msaga.1 ,
the accelerometer is calibrated at production level, and the calibration values are stored in the reserved registers, and it is better to not modify them.
However, it could happen that after the soldering process or handling actions, the accelerometer might be slightly out of calibration, and in this case you can:
If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster.
-Eleon
2021-04-28 7:15 AM
Hi Eleon,
Thank you for your answer. Regarding your suggestion to measure the offset on the 3 axis in a steady position, and write the obtained values in the X_OFS_USR (3Ch), Y_OFS_USR (3Dh) and Z_OFS_USR (3Eh) registers. I saw that the values on the axis at rest are not 0, but there is a slight deviation. What can I do so the values will be 0(except at Z of course that should be close to g value)
Thank you
2021-04-28 8:32 AM
Hi @Msaga.1 ,
you can characterized accurately these value and then put them in the register (volatile memory): when you'll run the acquisition, you'll get the already compensated values in the output registers.
You can do the same for the Z axis, but you have to subtract the 1g nominal value.
-Eleon
2021-04-29 2:47 AM
Thank you very much
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.