2020-01-17 4:24 AM
Dear friends, help me please solve the problem that I encountered during the calibration of the LSM303 DLHC magnetometer. I use the technical documentation stm32 AN3192 for calibration. After rotation of the sensor along each axis and data collection, correction factors for displacement and normalization are calculated. Given these coefficients, I should get a normalized sphere with a radius of 1. However, this does not happen. After that, I separately display the calculated values of the calibration coefficients. Can elements A, B, C be negative values?
Tell me what can be caused by their negative values?
Solved! Go to Solution.
2020-01-17 7:41 AM
Hi @ABogd.1 , they should not be negative because they define a sphere in space. Can you share the data you acquired? Did you already check the Motion MC library code of the X-CUBE-MEMS1 function pack, for the magnetometer calibration? Regards
2020-01-17 7:41 AM
Hi @ABogd.1 , they should not be negative because they define a sphere in space. Can you share the data you acquired? Did you already check the Motion MC library code of the X-CUBE-MEMS1 function pack, for the magnetometer calibration? Regards
2020-01-18 1:47 AM
Thank you very much for having promptly withdrawn my question. In the file, data taken from the sensor during rotation along each axis. It is from these data that I make the calculations.
I did not understand the application for magnetometer calibration, so I want to have an autonomous system with density.
2020-01-18 1:48 AM
Thank you very much for having promptly withdrawn my question. In the file, data taken from the sensor during rotation along each axis. It is from these data that I make the calculations.
I did not understand the application for magnetometer calibration, so I want to have an autonomous system with density.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.