2018-04-10 5:21 AM
Hi,
I'm trying the example software for the BlueCoin, also DataLog. The USB streaming of data is working the way it's written in a Start guide. But I'm not moving forward with DataLog on SD Card. I'm going through the following steps:
1. Setting LoggingInterface = SDCARD_Datalog in main.c
2. loading program onto BlueCoin
3. Connecting BlueCoin to Cradle, which is connected to battery and has SD in it.
4. Tapping on a board, the way it's written in a guide.
Result: nothing happens. When I open the SD Card folder, there's nothing to see.
I also tried different SD card, didn't help.
Does anyone have the same issue and could help me?
Thanks
#sdcard-logging #bluecoin #datalog2018-05-03 5:56 AM
Hi Natalia,
Could you please double check the following:
- you are using a micro-SDHC and not an old SD.
- you are doing a 'double tap' gesture to start the logging --> The LED should become brighter once active
If it still doesn't work you could try to use the binary provided within the package instead of recompiling it yourself.
en.stsw-stlkt01.zip\STSW-STLKT01_V1.3.1\Projects\SensorTile\Applications\DataLog\Binary\DataLog_SDCard.bin
2018-06-05 8:09 AM
Hi David,
I am using micro-SDHC card as you are saying.And I am able to upload the code as well on the bluecoin. When I press the button 2 to start logging data in the SD card. The LED1 remains on all the time.I was able to figure out that the problem which I was facing was that f_open function was giving me fr_disk_err. I didn't make any changes to the code that they have provided. Can you please help me with it? Thank you.I am using Nucleo-L073RZ for debugging and uploading the code.And then after uploading the code. I used the leds to find out the error while using sdcard (since we need to disconnect it from debugging hardware to attach sd card module.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.