MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LPR430AL roll angle wrong

Posted on August 07, 2012 at 14:38I work with the gyroscope LPR430AL. The pitch angle works fine, the roll angle results in some strange values... (if I turn the module of 90° in roll angle I measure the right value of 90°. When I come back to 0°...

iNemo Lite code's interface?

Posted on July 06, 2012 at 19:45I have the iNEMO Lite code for its Extended Kalman filter.  I have a board I made with an LSM303DLM and LSM330DL connected to the STM32F4 Discovery board for the IMU.Is there any example?  It looks like it's a library...

dannym by Associate III
  • 1113 Views
  • 1 replies
  • 0 kudos

Inprove the speed of the ''Mass storage'' as u disk

Posted on March 13, 2012 at 09:30hello everybody,  I was tested using the TF card as a U disk routines.The read speed is 500KB-700KB / s, write speed of 100KB/ s. Too slow, I would like to increase its transmission speed.I will change the way of the...

power3347 by Associate II
  • 5257 Views
  • 15 replies
  • 0 kudos

lsm330dl accelerometer output data problem

Posted on July 03, 2012 at 06:04i'm using the accelerometer in lsm330dl. but when i put the chip statically on the table, the xyz output i got from it is very strange,  for x, it's always between 0.2-0.45  for y, it's always around 1  for z, it's al...

LSM303DLM

Posted on September 08, 2011 at 11:23Hi all, I'm working with LSM303DLM. I have read successfully accelerometer and magnetometer value. Now, i want to use LSM303DLM module as a wakeup device. When my motorbike don't move, the MCU goes to Standby mod...

LIS331HH z-Acc is always zero

Posted on March 19, 2012 at 14:39Hi, i wanna access the acceleration values for the x,y,z axis. So i get a response and values from the registers x (0h28,0h29) and y (0h2A,0h2b), but the register for the z accelerations (0h2C,0h2D) is always zero. A...

iNemo firmware package v2.2.0 hex file

Posted on May 31, 2012 at 18:17Hi, I have been using for some time original iNemo suite application and DFU mode, then I made another program and uploaded it with JTAG programmer.How can I use iNemo suite again?, uploading iNEMOV2_Firmware_PackageV2...

miego by Associate
  • 1397 Views
  • 2 replies
  • 0 kudos

legal rights about SDK code

Posted on May 22, 2012 at 23:54Hi, is it allowed to upload the firmware of my custom inemo application (sportmeter), which based on the SDK of STmicro   to sourceforge ? WR Alex

sam239955 by Associate II
  • 2061 Views
  • 4 replies
  • 0 kudos

L3G4200D angle calculation

Posted on May 24, 2012 at 14:47Hi there,I'm using an L3G4200D sensor for calculating the angle displacementwith the code below. However from the computation I get half of the real rotationthe sensor make, that is, if I rotate it of 90 degree, I meas...

salvatore by Associate II
  • 1289 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.