LSM303DLHC as outdoor thermometer
Posted on December 11, 2013 at 08:06I want to use lsm303dlhc as outdoor thermometer. I use next code int8_t value= 25+data[0]; uint8_t sign=value&0x80; uint8_t cels=0; if(sign) cels=(~value)+1; else ...
Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
Posted on December 11, 2013 at 08:06I want to use lsm303dlhc as outdoor thermometer. I use next code int8_t value= 25+data[0]; uint8_t sign=value&0x80; uint8_t cels=0; if(sign) cels=(~value)+1; else ...
Posted on December 09, 2013 at 13:31Hello to all, In order to ease the self learning process and setup ST's LSM330DLC, attached to this post is an example of its drivers setup for a general application. Thank you, Thiago Reis #lsm330dlc
Posted on December 09, 2013 at 13:29Hello to all, In order to ease the self learning process and setup ST's LSM303D, attached to this post is an example of its drivers setup for a general application. Thank you, Thiago Reis #lsm303d
Posted on December 09, 2013 at 13:20Hello to all, In order to ease the self learning process and setup ST's L3GD20, attached to this post is an example of its drivers setup for a general application. Thank you, Thiago Reis
Posted on December 08, 2013 at 13:47Currently evaluating KIT EVAL DISCOVERY STM32F3. Where can i download IAR workbench for KIT EVAL DISCOVERY STM32F3.Thanks,
Posted on November 27, 2013 at 22:37I am trying to setup the LIS2DH to detect movement and drive INT1. The documentation is not clear what needs to be configured to do this. CNTL_REG3 appears to select the sources for INT1. There are two that are ...
Posted on November 27, 2013 at 14:38Hi, my INT1-Line is static low: with: response = LIS331DLH_SetIntHighLow(MEMS_ENABLE); // Interrupt active low; and response = LIS331DLH_SetInt1DataSign(LIS331DLH_DATA_READY); I get the data only about p...
Posted on August 09, 2013 at 23:45I have purchased the STEVAL-MKIO62v2 evaluation kit and I am looking for the source code so I can rebuild the firmware for this board. Essentially I need the source code for the RTOS that goes on the MCU as well as...
Posted on November 02, 2013 at 05:06The LSM9DS0 datasheet only appears to mention the accuracy of the accelerometer!?!? So the gyro and magnetometer have no accuracy specification? Please explain!!
Posted on November 12, 2013 at 08:34Dear Team.I need to read temperature data from LSM303DLHC for temperature compensation of the accelerometer data.I use the STM32F3Dicsovery board and the ''stm32f3_discovery_lsm303dlhc.c'' library. I can read the...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.