MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! lis2dux12 embedded advanced features page 2

Hi, I'm trying to decipher the inner workings of the fsm configuration on this sensor. While the an5904 application note features an example of configuration on page 42, things take a turn after the 21st step. The following step selects page 2, and I...

Resolved! LSM303AH mechanical shock support

Hello,  How many mechanical shock support the LSM303AH please ? and if uou have others reference of inclinometers thanks to give me informations. Thank you

ljm by Associate III
  • 1183 Views
  • 1 replies
  • 0 kudos

Resolved! LIS344ALH

Dear, Could you tell me if FS signal have internally pull up or pull down?   Regards

Stephslq by Associate
  • 2664 Views
  • 3 replies
  • 0 kudos

LSM6DSM Calibration not working by rotating 6 positions

Hi Everyone,I'm using STM32L4 with LSM6DSM on IAR IDE and using motion AC library to calibrate the accelerometer data. Code flow is like in first position when it has got the 500 samples for one position then it will wait till you rotate the position...

rshar.21 by Associate II
  • 805 Views
  • 0 replies
  • 0 kudos

Resolved! LPS22DF static addresses: 0x6B/0x6A or 0x5C/0x5D

We have a STEVAL-MKI224V1 kit, which should be equipped with a LPS22DF. I have tried to use the static (I2C) address of the sensor, and after much time, I discovered it is (depending on the state of SDO) 0x5C/0x5D, and not 0x6B/0x6A, as stated in the...

tcachat by Associate II
  • 2453 Views
  • 3 replies
  • 0 kudos

LIS3DH Excess Current Associated With INT1 Setup

Hello,We have implemented the LIS3DH with a nRF52832 in I2C mode on our board, and are using the accelerometer to detect motion and vibration events. The LIS3DH internal high-pass filter and threshold detection are used to generate the INT1 interrupt...

CBraun by Associate
  • 1780 Views
  • 0 replies
  • 0 kudos

LM6S3TR device FIFO pattern incorrect

Hi there!I'm having issues with my LSM6DS3TR device FIFO. I am trying to read and process all values stored in the FIFO by the accelerometer every interval using I2C. I am doing this by:1) Retrieving number of unread messages in FIFO at addresses 3Ah...

Programming MP34DT05-A MEMS DIGITAL MICROPHONE

Hello everyone,My goal is to record audio from one MP34DT05-A microphone via SAI PROTOCOL in an STM32F446 Nucleo Board. In resume, I receive data from microphone via DMA, then I make the transformation via PDM2PCM Library and write the buffer into an...

0693W000001r6oMQAQ.png
ALope.1 by Associate II
  • 3406 Views
  • 3 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.