MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STA321MP DSP + MEMS Mics Development

Posted on February 26, 2015 at 20:17Hi,I'm working on a personal project based on the STA321MP + MKI129Vx in order to record audio stream from an array of mics.Our first prototype was built on TI DSP but couple of months ago we decided to switch to ...

STA321MP DSP + MEMS Mics Development

Posted on February 26, 2015 at 20:17Hi,I'm working on a personal project based on the STA321MP + MKI129Vx in order to record audio stream from an array of mics.Our first prototype was built on TI DSP but couple of months ago we decided to switch to ...

No Range or Raw Value

Posted on June 10, 2014 at 18:20I am using a VL6180 as a proximity detector.  I am able to communicate the part without any issue, but when I read the RESULT__RANGE_VAL register or RESULT__RANGE_RAW I only read 0xFF with no target and 0x00 with a ta...

tekochip by Associate II
  • 4662 Views
  • 11 replies
  • 0 kudos

LSM303D FIFO operation

Posted on February 13, 2015 at 12:54Hi, I am developing an application using the LSM303D connected via SPI to continuously log the acceleration. I want to use the embedded FIFO to minimise the processor load but cannot find the correct configuration...

LIS3DH no Acknoledge

Posted on January 22, 2015 at 19:04Good morning,Our company is developing a vending machine that includes your sensor LIS3DH controled by one STM32 microcontroller. But until now we haven't get it to receive even the first acknolege response from th...

bfeixas by Associate II
  • 2417 Views
  • 1 replies
  • 0 kudos

LIS3DH Interrupts

Posted on February 24, 2015 at 13:08Hello,Is it possible to generate interrupts on relative acceleration variation, on LIS3DH?For example, I have my board on the desk and I'd like to generate an interrupt when I bump the desk. That should generate a...

George.P by Associate III
  • 1450 Views
  • 0 replies
  • 0 kudos

LIS2DHTR modes HI or normal resolution

Posted on February 23, 2015 at 23:33In the LIS2DH datasheet Table 28., the mode with ODR<3:0> = 0x9 .Is it possible to set a ODR of 1344Hz at a 12 bit resolution?Is it possible to set a ODR of 1344Hz at a 10 bit resolution? #odr #lis2dh

LIS3DH loosing sensitivity/calibration on power up

Posted on September 08, 2014 at 17:37We are using LIS3DHTR in our design. Supply voltage is 3.3v.  Due to capacitors in our design, it takes some time for the 3.3v supply to drain out completely. So, when we turn off and on the unit, there is a chan...

vemani by Associate
  • 1014 Views
  • 1 replies
  • 0 kudos

LSM330LDC SPI mode

Posted on January 11, 2013 at 18:05Section 6.2 of the data sheet says that ''SPC,SDI,SDO are common'' however there are 2 different SDO pins, SDO_A and SDO_G. Has anyone tried connecting the two SDO pins on the target board?  Does anyone know if I2C...

don2399 by Associate
  • 2102 Views
  • 3 replies
  • 0 kudos

Continuous acquisition from LIS3DSH

Posted on February 12, 2015 at 16:24Hello I'm attempting to acquire continuous data at high rate from a LIS3DSH, and getting discontinuities in the data - any input / suggestions / feedback would be hugely appreciated.  The aim is full rate of 1600...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.