MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LSM303D Z-axis Direction

Posted on March 23, 2015 at 23:28Why if the LSM303D a steady-state on a horizontal surface measures 0 g on the X-axis and 0 g on the Y-axis, whereas the Z-axis measures 1g = 1000mg?Direction of  Z detectable accelerations is upward (see pag. 8/52 Do...

LIS3DSH Power Down Current

Posted on December 05, 2014 at 21:12I only seem to be able to power the LIS3DSH down to about 70uA by writing a 0x00 to CTRL_REG4 (0x20). CS is High. SEL is Low. I am using I2C. Running at 2.5V What do I need to do to get to the spec power down curr...

sgetz by Associate
  • 1118 Views
  • 1 replies
  • 0 kudos

using self test feature of LIS3DSH

Posted on January 19, 2015 at 10:35how can i manage the self test in LIS3DSH.after enabling this option what i do? where can i found the result of  test?

LIS2DM I2C and low power

Posted on June 13, 2014 at 10:07after power up the LIS2DM the current consumption is about 100uA ?!The connection is:Pin1 : SCL with a external 4K7 to 3VPin2 : SDA with a external 4K7 to 3VPin3 : SA0 connected to GNDPin4 : /CS connected to 3VPin5: I...

SP Dirver interface for LSM303D

Posted on February 15, 2014 at 11:59Hi, I am looking for SPI driver interface for magnetometer LSM303D thanks #lsm303d-spi-driver

are there any ST mems engineers that know the LSM303??

Posted on March 17, 2015 at 13:38Does ST have any mems engineers?.... specifically an expert on the LSM303??? I'm having hardware issues with this part...(it is connected properly, board layout 100%, spi interface working.....not a hobby/hack deal.....

jyoung2 by Associate
  • 849 Views
  • 0 replies
  • 0 kudos

Nucleo F401RE , VL6180x issue

Posted on March 16, 2015 at 16:21The original post was too long to process during our migration. Please click on the attachment to read the original post.

STEVAL-MKI109V2 and STEVAL-MKI154V1

Posted on December 23, 2014 at 16:39I have installed UNICO v4.0 to acquire data from the STEVAL-MKI154V1 accelerometer/gyro. However, it seems I am unable to establish a connection with the evaluation kit. The STMicro Virtual COM Port appears in the...

Please fix LIS3DSH datasheet.

Posted on March 10, 2015 at 10:18It took me a while to understand it, but the datasheet for the LIS3DSH chip is dead wrong. It's a pretty obvious copy/paste mistake while creating that datasheet from another chip, but there is no such thing on that ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.