MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LSM303D is noisier than LSM303DLHC

Posted on December 05, 2014 at 00:07We are testing out the LSM303D in our new product and we are finding that it is a lo noisier than the LSM303DLHC.    Should this be the case? We assumed that the LSM303D would have less noise.Our init sequence;   ...

spi functions

Posted on January 13, 2016 at 19:51helloi use in stm32f4 with Keil uVision5 and STM32CubeMX(i cunfig spi with cubemx ).i want to send and receive data from accelerometerI can not find the SPI function that send/receive data because i search fanction...

spi functions

Posted on January 05, 2016 at 19:50halloi use in stm32f4 with Keil uVision5 and STM32CubeMX(i cunfig spi with cubemx ).i want to send and receive data from accelerometerI can not find the SPI function that send/receive data because i search fanction...

Write issues with CTRL_REG6_XL of LSM6DS0

Posted on January 11, 2016 at 11:04 Hi everybody, I have a custom board hosting anLSM6DS0 sensor and an STM32F427 micro which communicate via SPI. The SPI interface is configured as follow: SPI5h.Instance = SPI_MEMS; SPI5h.Init....

valerio2 by Associate II
  • 675 Views
  • 0 replies
  • 0 kudos

AdaPilot - Open Source Autopilot with ST Sensors

Posted on January 10, 2016 at 15:18Hello ST Community,I would like to share with you the exiting announcement of the imminent start of the open source project AdaPilot, a safety critical autopilot for unmanned systems (drones) based on the Ada-SPARK...

jarno23 by Associate
  • 837 Views
  • 0 replies
  • 0 kudos

LIS3DH reading axes values problem

Posted on January 06, 2016 at 07:42I'm using LIS3DH_driver project from ST to read axes values from LIS3DH accelerometer. I'm not using STM32 but I have implemented my own LIS3DH_ReadReg() and LIS3DH_WriteReg() functions somehow and they are working...

AIS328DQ - Spurious incorrect measurements

Posted on December 31, 2014 at 08:09 Hello all, I'm having trouble using the AIS328DQ accelerometers. Having the board level I should get roughly 0,0,1 for the x,y,z axis. Every second or third reading is completely incorrect. Often it's...

samuel2 by Associate
  • 731 Views
  • 0 replies
  • 0 kudos

VL6180X performance

Posted on December 30, 2014 at 16:47The application is simple - proximity detection between 20mm and 150mm. The VL6180x is clear (no glass or any other surface covering the sensor)I tried to initialize both with the default values of the VL6180X and...

sound synthetesis

Posted on December 30, 2014 at 10:31helloI'am trying to develop an application for voice synthesis using STM32 F4 discovery .for this work i used the project Audio_playback_and_record .however,when i modified the PCM code of const uint_16 AUDIO_SAMP...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.