MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS3DSH Calibration

Posted on July 04, 2016 at 08:11Dear ST engineer,I use LIS3DSH for digital angle meter development.But I have calibration error on LIS3DSH.I am study ST DT0053 6-point tumble sensor calibration.Could you give me a calculation example for the sensor ...

LIS3MDL selftest and calibration

Posted on June 16, 2016 at 13:24Hi,the self test procedure described in AN4602 starts automatically by setting bit 0 to '1' in CTRL_REG1 register, but it is not well explained how to check if the self test passes or fails.If the self test passes, th...

marziano by Associate
  • 2603 Views
  • 2 replies
  • 0 kudos

Problems Calibrating Motion FX

Posted on June 23, 2016 at 23:53I have read over the user manual for the MEMs board, and I am using the example code from the DataLogFusion. However, I can never get the osx_MotionFX_compass_isCalibrated function to return true. I have tried hitting...

hushel by Associate II
  • 1199 Views
  • 1 replies
  • 0 kudos

LSM330DLC I2C

Posted on January 28, 2016 at 13:10Dear All,I am using LSM330DLC gyro-acc on my board and I have forgotten place pull-up resistors on the SPI/I2C selection pins. However it works fine. My question is can I develop my project without these pull-up re...

IIS2DH data convert data to g

Posted on June 06, 2016 at 03:14I'm using IIS2DH, I config it to normal mode, so It's 10bit resolution, and I got 16bit data for each axis, now I right shift the 16bit data to get a 10bit data, and the range is 0-1023, is that right? but And if I k...

LIS3DHTR interrupt pins

Posted on May 25, 2016 at 14:09Hello guys, I'm planing to use LIS3DHTR accelerometer in my next project. There is one thing (for the moment :-)) that is bothering me: The default state of the INT1 and INT2 pins is not explicitly indicated within a d...

bojan by Associate II
  • 1055 Views
  • 1 replies
  • 0 kudos

STEVAL-MKI159V1 connection to Raspberry PI 3

Posted on May 25, 2016 at 18:57Hello everyone. This is my first posting on this forum. I am an electrical engineering major completing a senior design project. I am designing a smartwatch and I purchased the STEVAL MKI159V1 motion sensor and this wi...

jigle004 by Associate
  • 993 Views
  • 1 replies
  • 0 kudos

Sensor Controller Studio with LPS22HB

Posted on June 27, 2016 at 15:50Hi everyone,I'm working on LPS22HB and I use Sensor Controller Studio (a TI's tool).Do anyone in this forum used this Studio? We can exchange knowledge and experience. Best,Dung. #lps22hb #ccs #scs

le by Associate II
  • 831 Views
  • 0 replies
  • 0 kudos

Downscale range

Posted on June 23, 2016 at 05:04Is it possible to down scale the range by 2 to 50mm and output in 0.5mm increments represented as integers in a similar way upscaling works?

USB AUDIO DRIVER QUESTION

Posted on June 22, 2016 at 16:17 Hi guys, Sorry that I have a dumb question I am new to STM32's board, and we are currently using  F446 with MEMS microphone module. We want it act as a USB microphone like what it said.   http://www.st.com/content...

cks7788 by Associate II
  • 605 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.