MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Half sensitivity of one VL53L0X

Posted on November 07, 2016 at 11:56Hy,for a proof of concept I created five identical devices, each having 3 VL53L0X, so I have an overall of 15 VL53L0X that are mounted (behind an acrylic glass shade) and connected (via 2.8V, I2C) identically. Dur...

harald by Associate III
  • 823 Views
  • 2 replies
  • 0 kudos

Is the LSM6DS3H and LSM6DS3US the same part?

Posted on February 22, 2017 at 02:00I have went to just order the H version and found there is none left. Anywhere. So then I started looking and the US version is on stock. All the specs look identical but I just want to know for sure. Any help or ...

curtis2 by Associate
  • 1021 Views
  • 1 replies
  • 0 kudos

wesu ResetManager, UsbDfu and OtaDfu

Posted on February 21, 2017 at 18:22Hello,in wesu downloads I can find ResetManager, UsbDfu and OtaDfu applications in bin format.Are they available also in source format?Thanks in advanceFabiano

fabiano by Associate
  • 617 Views
  • 0 replies
  • 0 kudos

Connecting the API with STM32 platform in CubeMX

Posted on February 13, 2017 at 16:04HiIm having the device VL53L0X which I want to communicate with trough the I2C protocol to my STM32F401RE micro controller.Im using CubeMX from STM to setting up the pins which works fine, but I don't know how I '...

VL6180X max convergence error

Posted on November 11, 2016 at 10:45I always get the error 0b0111 (max convergence) if I make a range single shot measurement (I also don't know if other modes are working). I tried to disable the ECE but still the same. I tried it with the code fro...

Lifting and teft detection by LIS2DH

Posted on February 20, 2017 at 08:57Hi,I am using LIS2DH in our custom board and I am trying to detect some scenarios using this accelerometer. I read the datasheet and application note and tested almost all features. But I'm not sure how to apply t...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.