MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STEVAL-IDB007V1, old usb serial fw detected, OLD DTM FW detected

Posted on April 02, 2017 at 12:47Hi All,I am using STEVAL -IDB007V1 development KIT, i installed BlueNRG GI c2.2.2, when i try to connect to the device(click connect), i am getting 2 messages:1-  old usb serial fw detected.2- OLD DTM FW fw detected....

Nav Dev by Associate II
  • 659 Views
  • 0 replies
  • 0 kudos

53L0-SATEL problem

Posted on March 23, 2017 at 13:25I'm having some troubles using the VL53L0X sensor (53L0-SATEL-I1 board); I used the other satellite board included in the x-nucleo-53L0A1 without any problems, but the 53L0-SATEL-I1 isn't working properly; it seems t...

LSM9DS DEN_A/G

Posted on March 29, 2017 at 18:10Hello,How could I enable the DEN_A/G signal?I succeeded to enable the DRDY_M or INT1_A/G signal but I have nothing on this DEN_A/G.Do you have any suggestion?Best regardsMich

Mich1 by Associate III
  • 1151 Views
  • 4 replies
  • 0 kudos

LSM303AGR how to get 12-bit resolution on accelerometer

Posted on March 28, 2017 at 20:03LSM303AGR how to enable high resolution mode on the accelerometer? I have done exactly as described in the data sheet/manual setting the LPen bit to 0 and the HR bit to 1. I can play around with these bits but it doe...

STEVAL-STLKT01V1 to command a motor

Posted on March 27, 2017 at 18:19Hello, I am currently working on the STEVAL-STLKT01V1 development kit and I would like to use the sensortile to give an analog output in order to activate a motor. Does anyone know which of the output pins of either ...

VL53L0X freeze after ~1 min of use

Posted on March 21, 2017 at 23:05Hello,I am trying to operate the VL53L0X through ADLINK I2C SEMA3.5R7 (com express) interface.I initialized all the registers correctly according to - https://github.com/pololu/vl53l0x-arduino/blob/master/VL53L0X.cpp...

LPS25H wrong pressure value

Posted on July 27, 2015 at 18:07 Hi ST Community! I am working with LPS25H pressure sensor and STM32F1 uC. I am able to read out temperature and pressure but the pressure value is too low (temperature is fine). It should be 15 mbar and t...

zlajoan by Associate II
  • 2589 Views
  • 8 replies
  • 0 kudos

H3LIS200DL I2C not working for more than 5 mins

Posted on March 20, 2017 at 13:40Hi, I am using H3LIS200DL with RFduino (RFD22102 ) as microntroller, I have used the schematic given in data sheet except I have connected CS pin to Vdd (for using I2C). Also I am using Arduino H3LIS331Dl_demo code a...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.