Resolved! FSM double tap
Hi, I'm trying to implement the tap and double-tap function in the FSM tab. Is it possible to achieve this at an output data rate of 26 Hz?
Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
Hi, I'm trying to implement the tap and double-tap function in the FSM tab. Is it possible to achieve this at an output data rate of 26 Hz?
We are using the X-STM32MP-GNSS2 (with the STM32 discovery board DK2), which has ISM330DHCX IMU. The accelerometer readings seem fine from the IMU, but the gyroscope gives enormously high and varying readings even when we are stationary. See below th...
Hi all!I've recently started working on a fault classification model utilizing the proteus1 board and the NEAI studio suite. I'd ideally like to set up a serial datalogger via the onboard micro USB to both obtain and display readings, alongside bench...
Hello, I'm currently working on ST1VAFE6ax sensor to read 6 axis data from accelerometer and gyrometer via SPI protocol. But sensor is not behaving as expected. it returns the value as 0. Is there any initial booting process for the sensor or is anyt...
We embed LIS3MDLTR on our board that we produce, because this has high sensitivity: 6842 LSB/gauss. This corresponds to 0.146 mgauss/LSB, if I convert correctly. The other products has significanltly lower sensitivity: 1.5 mgauss/LSB. What are you pr...
Dear ST/Forum,We are using the LPS22HBTR pressure-temperature sensor in some PCB assemblies.Due to some cleanliness requirements of the experiment, I need to be able to clean the PCB this device is attached to but due to the very fine holes in the li...
Thank you for solving my problem. Please forgive my poor English.I am using lsm6dsl sensor. When I use FIFO to read LSM6DSL, the data is correct at the beginning, but later there will be data errors. configuration :XL_ODR_208HzGY_ODR_208HzFIFO_208Hz2...
Are there any plans to have a video tutorial on the biosensor eval board? (ST1VAFE3BX)? I connected it to MEMS Studio via the MKI109V3. I'm experimenting with the "Features Demo" but it's not behaving as I expect. Perhaps there's documentation abo...
I am using Mems-Studio for my FSM project. I am testing the state machine, and everything is working fine; I can see interrupts. However, in the debug tab, when debug mode is enabled, the table does not compile, and I cannot observe the program's beh...
Dear ST/Forum,Preamble:We are using the LPS22HBTR pressure-temperature sensor in some PCB assemblies.The data sheet indicates a pressure reading range with defined accuracy from 260 to 1260hPA/millibar and an absolute maximum overpressure value of 2M...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.