MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS2DW12 sensor FIFO not working properly

Hi,We are using sensor LI2DW sensor in our project. Sensor is connected to MC using SPI interface. We have configured the device as below.fifo en 0x3fodr sample rate : 50 hz.we are reading data every 500 msec, so we are expecting 25 - 26 samples of x...

Read data from gyroscope LSM6DSO using IKS01A1

I'm trying to read data from gyroscope. I set ctrl2_g and I'm trying to read 6 bytes from register address 22h. But in result I receive only 0 values. /* USER CODE BEGIN 2 */   LSM6DSO_CTRL2_G(&hi2c1, LSM6DSO_CTRL2_G_ODR_XL_833Hz, LSM6DSO_CTRL2_G_...

0690X000006CUonQAG.png
AJab� by Associate II
  • 1377 Views
  • 2 replies
  • 0 kudos

Accelermometer Range setting in ISM330DLC

Hi All,I am working on a project that is using ISM330DLC sensor for measuring the acceleration along the X,Y and Z-axis. When I set range 2G,4G and 8G I'm seeing difference in the sensor raw value and when I set it to 16G, I'm getting same data as 8G...

Resolved! LIS2DH internal sampling vs sample rate

Hi ST,I'm wondering about the sample rate of the LIS2DH* family and if the configured sample rate affects how the samples are captured. Specifically, when sample rate is changed, does that change how the samples are performed internally, or does is i...

pa.9 by Associate
  • 1696 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.