MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-Nucleo expansion board for LSM6DSO?

Hi, is ST planning to release new version of the X-NUCLEO-IKS01A2 sensor expansion board with the newest recently released sensors? I would like to interface LSM6DSO with NUCLEO-L4. Tks

f87 by Associate II
  • 784 Views
  • 0 replies
  • 0 kudos

LSM6DSO no interrupt

I have a LSM6DSO and I want to test it with the data ready interrupt, but I don't get any. I am using a logic analyzer to monitor the interrupt.The registers that I set are:0x18 with value 0x010x0B with value 0x010x10 with value 0x400x0D with value 0...

Resolved! H3LIS331DL: Threshold levels

I have the FS bits set for +/-100g scale.The accel data is a 12-bit signed value, meaning each bit represents 0.049g.The threshold registers however is only a 7-bit value. From what I understand, this is to be an unsigned magnitude level, representi...

RDyla by Associate II
  • 1840 Views
  • 3 replies
  • 0 kudos

How to use pdm to pcm conversion library?

I am working on a project where I need to calculate the ambient noise in a given environment in decibels, for that purpose I am using st microelectronics's MP34DT01-M microphone which has an digital PDM output. From the stm application notes I got t...

SHire by Associate
  • 1658 Views
  • 2 replies
  • 0 kudos

IIS2DH sensing Die Location

Where in the 2x2 package is the sensing die for the 3 axis located? Is it dead center? A technical answer as accurate as possible would be best. And if there is some known manufacturing variance ​of this location. ​T​hanks

Interrupt generation for activity event

Hello,I have configured LIS2DH12 to generate interrupt on INT2 pin on activity as well as a strong impact using the register values as follows:CTRL_REG1 - 0x37CTRL_REG2 - 0x00CTRL_REG3 - 0x40CTRL_REG4 - 0x88CTRL_REG5 - 0x0ACTRL_REG6 - 0x28INT1_THS - ...

AB.4 by Associate II
  • 728 Views
  • 0 replies
  • 0 kudos

LSM9DS1 magnetic sensitivity

Posted on July 10, 2018 at 16:40The magnetic sensitivity for the LSM9DS1 is 0.14 mguass/LSB on its most sensitive range.  The LIS2MDL is 1.5 mguass/LSB.  Is the LSM9DS1 really 10X more sensitive?  If so, it would seem the best choice for application...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.