Where are the cutoff frequencies of the accelerometer highpass filter?
Hello everyone,Table 71 contains the cutoff frequencies of the low pass filter, which depend on the ODR. There is no similar table for the highpass.Thanks in advance
Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
Hello everyone,Table 71 contains the cutoff frequencies of the low pass filter, which depend on the ODR. There is no similar table for the highpass.Thanks in advance
I want higher data rate for magnetometer from LSM9DS1, specifically 100Hz.I found 'FAST_ODR' option in CTRL_REG1_M register but couldn't find any details such as side-effects or maximum ODR.Where can I find documents for the FAST_ODR? Or is it just i...
Hi,We have recently purchased the STEVAL-BFA001V1B kit and planned to connect the STEVAL-IDP004V1 to the STEVAL-IDP005V1 as we planned to use the STEVAL-IDP004V1 GUI interface to allow for streaming off data from the sensor.The manuals we have used a...
Dear Sir/Madam,we have recently purchased the STEVAL-BFA001V1B kit and planned to connect the STEVAL-IDP004V1 to the STEVAL-IDP005V1 as we planned to use the STEVAL-IDP004V1 GUI interface to allow for streaming off data from the sensor.The manuals we...
Hi,We have recently purchased the STEVAL-BFA001V1B kit and planned to connect the STEVAL-IDP004V1 to the STEVAL-IDP005V1 as we planned to use the STEVAL-IDP004V1 GUI interface to allow for streaming off data from the sensor.The manuals we have used a...
I'm trying to implement a self-test for the LSM6DSOX in Mode 1 (as in page 118 of AN5272 Rev 3). Could someone explain what the ST_X, ST_Y, ST_Z variables represent? Would Min(ST_X) be the minimum value of the 5 samples while self-test is enabled, or...
Hi,I'm trying to configure the AWT function in the LSM6DSL. All works fine minus the latency. I change the latency to 0x01(40ms) but the interrupts keep with a delay of 600ms(default) between each one. Any idea what I'm doing wrong?Accelerometer band...
Is there any simulation software available for IMU sensors where can I attach the circuit of IMU IC sensor with the STM32 development board?
For example, IIS2MDC's sensitivity is 1.5mgauss/LSB. How much is the min angle change or position change can it measure? How much is the difference between 1.5mgauss/LSB and 1mgauss/LSB?
I use the example project X-CUBE-53L0A1. The problem is that this project hasn´t a device configuration tool. Is it possible to add this tool to the project?Example Project Source:https://my.st.com/content/my_st_com/en/products/ecosystems/stm32-open-...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.