MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LSM303DLHC heading calculation

Hello everyone. I have been struggling with creating the tilt compensation compass. I have prepared the code which is based on demo firmware but I don't receive reliable output. I mean, when I rotate the development board, the heading value doesn't l...

Mems Library IKS01A3 e-compass

Hello eveyone, I used LSM6DS3 mems that I would like to get quaternion data, without MAGNETIC. Can I use MotionEC_Run function and without MAGNETIC?And then, I try to run MotionEC_Run(&data_in, &data_out) function under the STM32CubeExpansion_MEMS1_...

LSM9DS1 Library

Who knows where can get LSM9DS1 Library for STM32?I ever find the X-CUBE-MEMS Library, but I didn't find LSM9DS1 library. And then, If it can use, but its magnetometer different to X-NUCLEO-IKS01A3of LIS2MDL. How should modify by its library?

Reading HALL Sensors values from HALL interface

Hi dear members, I am trying to understand complete how to drive bldc motor.And I would like to use hall interface in stm32.how can I manage to read commutation using hall sensors which registers I couldn't find it in reference manuel.And also how ca...

Zek_De by Senior
  • 4889 Views
  • 6 replies
  • 0 kudos

STM32CubeProg failed to download FP-AI-SENSING1

Hello,STM32CubeProg outs "Error: failed to download Segment[0]" and failed to download FP-AI-SENSING1(SENSING1.hex).My envs are,SensorTile kit with small cradle.The FP-AI-SENSING1 ver.3.0.0The project is imported from SW4STM32 to STM32CubeIDE ver.1.0...

Yuk117 by Associate III
  • 2005 Views
  • 1 replies
  • 0 kudos

HTS221 and condensation

The HTS221 has an internal heater to "speed up the sensor recovery time in case of condensation".How do I identify a condensation state?How long the heater has to be activated, in order to recover from condensation state (I want to estimate power con...

GShim by Associate II
  • 2519 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.