MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SensorTile.box #2: One structure, infinite applications

Have you ever wondered how to build a plug-and-play barometer, or a pedometer, or even a vibration monitoring? This is almost immediate with a SensorTile.box. Once the BLE connection is set-up and the last FW has been downloaded, the Example app scre...

0690X00000ARY5pQAH.png

LIS2DW12/LIS2DTW12 OCR Timing Accuracy

Regarding the LIS2DW12 and LIS2DTW12 devices, there is no published specification on the accuracy of the ADC sampling frequency in the datasheet, nor it's drift against temp and supply voltsage. Without these data the selected ODR is a guess, e.g. 40...

AMoul by Associate II
  • 1531 Views
  • 3 replies
  • 0 kudos

Zero-g values for IIS2DH

I am using IIS2DH accelerometer for vibration analysis. As per the datasheet the Zero-g level for x and y axis is 0 while z axis measures 1g. For my application when the device is resting x and y shows zero but z shows the value which give wrong read...

YMand.4 by Associate
  • 1203 Views
  • 2 replies
  • 0 kudos

LSM6DS3 fifo read via i2c

I have been reading a 780 samples from lsm6ds3 FIFO via i2c (i2c_dev driver from linux) but the read is taking arround ~1.5 to 2 sec. this seems little unusual to me . is there any way to reduce the i2c read time ?.Here is my read function:static int...

thejas by Associate II
  • 1609 Views
  • 2 replies
  • 0 kudos

About the LPS22HH' s temperature compensation

HiWe are testing the LPS22HH on the MKI192V1, and we have got the pressure and the temperature. We also convert the pressure value to the height.We put the LPS22HH in the metal shell, and It is not sealed. We use air guns to heat the shell, and we fi...

User.120 by Associate II
  • 1693 Views
  • 2 replies
  • 0 kudos

LIS331 output is not stable

Hi Guys,I encountered a very strange problem and hope you can give me some suggestions!The LIS331 is adopte to measure device tilt, we assembled the PCBA in vertical positon and this means the sensor also works at vertical status. Please see the atta...

0690X00000ARGfVQAX.jpg 0690X00000ARGfLQAX.jpg
DJohn.6 by Associate II
  • 2364 Views
  • 5 replies
  • 0 kudos

[LSM6DSM] How to properly setup basic readout

Hello,I'm struggling with LSM6DSM readout and would like to ask for some insight. I use a custom board with 7 other I2C sensors and the LSM6DSM is the lost one I need to handle. Among them is a H3LIS331 from ST.For all of them I use the same code for...

AR2 by Associate
  • 1658 Views
  • 2 replies
  • 0 kudos

SW design of interrupt for lsm303ah

Hi,I'm Looking for a suitable design pattern to reliably handle interrupts from the embedded functions, i.e. pedometer, tilt and significant motion.Kind regardsJerker​

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.