MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to program/flash STEVAL-BLUEMIC-1

How do I flash the STEVAL-BLUEMIC-1 board? The STEVAL-BLUEMIC-1 board came with a 5 pin SWD programming cable. What does this interface with? Is there an ST Link tool that connects to the SWD cable and a USB port on a computer?

SHack.1 by Associate II
  • 4620 Views
  • 9 replies
  • 0 kudos

Resolved! How to setup the STEVAL-MKI211V1K

Setup is for the accelerometer STEVAL-MKI211V1K. My laptop is HP Folio 9480m using Window10. Laptop connecter through USB cable to the STEVAL-MKI109V3 running UNICO software. USB Virtual COM port was successfully setup on COM6, on the STEVAL-MKI109V3...

LStoh.1 by Associate
  • 3455 Views
  • 3 replies
  • 0 kudos

LIS3DHH SPI mode?

Can someone confirm which SPI mode (0 thru 3) LIS3DHH uses?It is not explicitly mentioned and from the diagram it seems to be either mode 2 or mode 3 (which start with clock high), but then I'm not too sure.

Resolved! How to configure the sensors of STEVAL-STLKT01V?

Hello everybody, I'm working with my SensorTile development kit (STEVAL-STLKT01V1) for a short time now and I'm trying to get it working. I can connect to the sensor board via bluetooth using my iphone and the ST BLE Sensor App and on the PC (Win10) ...

JStep.1 by Associate
  • 1842 Views
  • 3 replies
  • 0 kudos

Resolved! SensorTile.box Firmware upgrade

Hi everyone,I have been stuck at a problem. Initially i tryied to upgrade the firmware on SensorTile.box through the ST BLE Sensor App with some demos without any problems.Once i tryied to upgrade the BLEFOTA_BL_1.0.0.bin file through the app, so, wi...

EDimr.1 by Associate
  • 3103 Views
  • 4 replies
  • 0 kudos

Resolved! Peak detection on a LIS3DSH gives 0

Hi, I am working on a MEMS LIS3DSH connected via SPI to a STM32F207ZG having the following configuration:Full scale: 2gOperating mode: 100HzFilter: 800HzRegisters:CTRL_REG3: 0x48 (Interrupt pulsed, active high)CTRL_REG4: 0x6F (BDU enabled, XYZ enable...

0693W000004JGVEQA4.png
SMeye.1 by Associate II
  • 2257 Views
  • 5 replies
  • 0 kudos

Debug the Audio_SD example with Cradle mounted

Hello to everybody,I bought the bluecoin evaluation kit and I'm interested in logging audio data in SD, similarly to the Audio_SD example.I have tried the Demo, downloading the .bin using the SWD cable from the nucleo board. Then removed the CoreSyst...

frnt by Senior
  • 1082 Views
  • 1 replies
  • 0 kudos

Sensortile box not visible at bluetooth profile

Its quite stressful to see the sensor box not working. It hangs with demo apps. It tried to connect repeatedly while plotting data when it was working. Have used it only for a day. After firmware update, it does not respond. Blue LED does not blink a...

SGupt.4 by Associate II
  • 3969 Views
  • 8 replies
  • 0 kudos

Resolved! Connecting two sensors to the same SPI bus - possible contention

Hi, In our system there's an LSM6DSL accelerometer and LPS22HH barometer connected to the same SPI bus.When nCS of the accelerometer is asserted (0), the nCS of the barometer is de-asserted (1) and vice versa.HOWEVER, as nCS=1 (for both sensors) als...

ELask.1 by Associate II
  • 2116 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.