MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS2DU12TR accelerometer

Hi,I am trying to use the LIS2DU12TR's low address that is 0x18 but I keep on encountering issues with not able to read WHO_AM_I and the accelerometer does not work. Can anyone please help me with this?Also, does it support 100kHz I2C bus?Thanks.

PE4A by Associate
  • 3354 Views
  • 3 replies
  • 0 kudos

Resolved! Problem with Resetting LSM303AGR sensor

 Hello everyone,I am using I2C to communicate between an STM32F411 Discovery Board and the on-board LSM303AGR sensor. I have already configured it for a 400Hz ODR, normal power mode, and am reading temperature values (around 25°C to 27°C).However, I ...

Resolved! Trying to make lis2dh sense any rotation

Hi, I was trying to make the sensor sense slow rotation.I read the datasheet and I guess if I set HPM to work as normal mode, and High-pass filter for interrupt 1so CTRL_REG2 should have 0x81,Then I should read the REFERENCE (0x26) register, (accordi...

abdu21 by Associate
  • 414 Views
  • 1 replies
  • 0 kudos

Resolved! ASM330LHH Initialization Procedure

Thank you for your continued support.From your responses, I have made the following initialization procedure for ASM330LHH.POWER ONCTRL3_C <- 0x42(BDU,IF_INC)CTRL1_XL <- 0x9C(3333Hz,8G)CTRL2_G <- 0x92(3333Hz,125dps)INT1_CTRL <- 0x01(Accelerometer dat...

ggob by Associate III
  • 1226 Views
  • 4 replies
  • 0 kudos

Resolved! LIS3DH simultaneous free-fall interrupt and normal XYZ operation

HiIs it possible to configure the interrupt function for free-fall with normal XYZ polled operation, or is it better to use the interrupt in low power mode and performing the free-fall via normal XYZ programmatically in normal operation?Thanks! 

rep by Associate II
  • 1013 Views
  • 4 replies
  • 2 kudos

Resolved! About Embedded compensation for ASM330LHH

Regarding the statement in the ASM330LHH datasheet “Embedded compensation for high stability over temperature”, does this mean that each output is temperature compensated? Does the compensation value correspond to the memory contents loaded when the ...

ggob by Associate III
  • 791 Views
  • 2 replies
  • 0 kudos

Resolved! LSM6DSOX high power consumption

Hello, I recently integrated LSM6DSOX on a testing PCB which contains an MCU and some other peripherals. The problem is that I have been trying to reduce power consumption without success, and I thought maybe you could help me find the problem. First...

dimitra by Associate
  • 730 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.