Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
Hello,I'm working with blueVoice over sensorTile.I downloaded FP-SNS-ALLMEMS2 project version 2.1.0 and also project FP-SNS-ALLMEMS1 in version 4.2.0 and 4.1.0On Android side i'm using ST Ble Sensor app from Play StoreAll of them give me a very bad a...
We are exploring MP34DT05TR microphone for our new product. If we connect flying wires on soldering pads then it works fine. But when we have hand soldered it on STEVAL-MIC001V1 PCB (Gerber of this PCB available on ST website), it is not working. We ...
Hi.For accelerometer LIS3DHTR, the output signals INT1 and INT2, pins 11 and 9, they are both push-pull (CMOS) outputs? or one of them, or both, have open-drain configuration?For my projects it is better that both INT1 and INT2 be CMOS outputs.Regard...
I've been working with a LPS28DFWTR pressure sensor and noticed it's pretty sensitive to sunlight. As in, the pressure will climb significantly when the sun shines on it. Because the membrane appears to heat much faster than the temperature sensor it...
can u help me fix this issue? sometime it gives alert when there is no noise
We've been using the LSM6DS3 for several years, and are considering a switch to the LSM6DSM. It appears they are pin-compatible, and a superficial look at the register descriptions indicates they could be software-compatible as well, i.e. I could swa...
Hi,I'm trying to do reset set in my lsm6dsox sensor. (I use stm32wbx, stm32cubeide,bucemx)İ wrote driver functions.When i get to initialization for my single_tap api . i can not get the default value from the sensor register.what can be the reason ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.