MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to transmit more than 8bytes data via basic CAN Bus

Hi all!I have a problem with transmition/receiving more than 8 bytes of data between two STM32 MCUs via CAN-Network.I know, it is impossible to transmit more than 8 bytes of data via basic CAN Bus.I tried to create Command messages System.CAN Master ...

USolar by Associate III
  • 7478 Views
  • 9 replies
  • 0 kudos

The VL53L0X‘s 0x83 address read content is 0x0.

I bought a  VL53L0X sensor, and download a example(it named vl53l0x-arduino-master) about it from github. And i found that the program stays consistent in the while ,as shown in the picture.So i want to ask the question is that why the 0x83 address r...

0690X000008BAw0QAG.jpg 0690X000008BAxIQAW.jpg
Xjihe by Associate
  • 1495 Views
  • 1 replies
  • 0 kudos

Official library for LIS3DH with FIFO DMA transfer

HI, I am trying to develop a application with a accelerometer over 5kHz.I have some samples of LIS3DH. Does exits any repository of mem senc?I search in cubemx but is not there.I can write the library from datasheet but it is a lot of time and it wil...

tcg by Associate III
  • 6290 Views
  • 6 replies
  • 0 kudos

H3LIS100DL static sensor detecting variable acceleration.

 resources: datasheetLibraryExample codeI am using the H3LIS100DL accelerometer with the default h3lis100dl_read_data_polling.c example, and can read it's output, but the acceleration varies while the sensor is static: When placing the H3LIS100DL st...

cr.1 by Associate
  • 1220 Views
  • 0 replies
  • 0 kudos

Resolved! Turnkey gesture recognition STSW-IMG035 library port to RISC-V Chips

Is there anyway to port the libGesturesMZ.a library to RISC-V or provide source code for this? Currently only can be used with Arm Cortex chips and we want to be able to use the VL53L5 sensor with Risc-V chip the standard code to operate VL53L5 is pr...

Baze by Associate II
  • 2703 Views
  • 3 replies
  • 0 kudos

About this video "Arduino tutorial: using Arduino Nano RP2040 with our new LSM6DSOX inertial sensor with embedded AI" , can we do the same process in a ESP32 and based on a external board like adafruit 4438 ?

It is possible to apply the same workflow to LSM6DSOX as show in the video "Arduino tutorial: using Arduino Nano RP2040 with our new LSM6DSOX inertial sensor with embedded AI", but with a ESP32 and a external sensor board like adafruit 4438 ?

JCanais by Associate
  • 1798 Views
  • 1 replies
  • 0 kudos

Resolved! HAL_I2S_Receive gives incorrect data

Hi!I'm trying to get an SPH0645 microphone to send sound data to my STM32F411 with HAL_I2S_Receive(), but the data I receive is not correct. According to the data sheet, the microphone gives 24 bits data on a 32 bit frame, with 24 bits containing dat...

0693W00000aITeFQAW.jpg 0693W00000aIThiQAG.png
Chasar by Associate
  • 3225 Views
  • 3 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.