MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32G474RE Internal temperature sensor returning very low value

HiI am trying to make work the internal temperature sensor from a STM32G474RE and it seems to return a low value... 11.14 celsius degrees.This is the code I am using:#define TS_CAL1_ADDR ((uint16_t*) ((uint32_t)0x1FFF75A8)) #define TS_CAL2_ADDR ((uin...

_legacyfs_online_stmicro_images_0693W00000bjQERQA2.png _legacyfs_online_stmicro_images_0693W00000bjQEWQA2.png
RPG by Senior
  • 3121 Views
  • 3 replies
  • 0 kudos

LIS2DW12 Bias issue

Hi MEMS experts,I am using LIS2DW12 to measure the movement with very rough distance.I tested it by measuring the X-axis only, but it seems to be biased to positive direction.I mean, Moving it to the positive direction : it starts having the + accele...

IIS2MDC read X,Y,Z, temperature via I2C - separately or together ?

I have the IIS2MDC along with LSM6DSL accel / gyro on a board with stm32L451 uC.Accel / gyro work fine. uC reads status byte then if any axis has new data ready it reads all from temp to accel (0x20-0x2d) in 1 ST hal fn call multi byte read: HAL_I2C_...

CClen by Associate
  • 2727 Views
  • 2 replies
  • 1 kudos

What's the best way to complete self-test on ASM330LHH?

I have followed the description in <an5296-asm330lhh-automotive-inertial-module-digital-3d-accelerometer-and-digital-3d-gyroscope-stmicroelectronics.pdf> to write self-test code, but the Accelerometer and Gyroscope's data is still not in the correct...

Xie1 by Associate
  • 1419 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.