STEVAL-MKI185V1 adaptor
Hi, I have STEVAL-MKI185V1 adaptor. For reading the data, i use 3 commands(*setdbxxxvy, *start, *mrAA). and then i can read only '1' data. How do i read continuous data? what 'command' i use for reading continous data?
Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
Hi, I have STEVAL-MKI185V1 adaptor. For reading the data, i use 3 commands(*setdbxxxvy, *start, *mrAA). and then i can read only '1' data. How do i read continuous data? what 'command' i use for reading continous data?
I'm looking to organize a POC centered around using VR/AR platform to measure disturbances on a human eyeball. This company URL seemed interesting.https://www.st.com/content/st_com/en/about/innovation---technology/mems-scanar.htmlI'd like to clarify ...
Hello, guys!Could you help us understand the issue with single data conversion for an internal temperature sensor of LIS2DW12? While experimenting we followed datasheet (DS11811 - Rev 8), Application Note AN5038 and single data conversion app note DT...
Hi,I have STEVAL-MKI185V1 adaptor. ST Microelectronics is already giving the software. But I would like to integrate the output from the motherboard through LabView. Can someone please tell me whether it is possible to use LabView as acquisition soft...
We are planning to use ASM330LHH at a distance of about 1m from the MCU to which it will interface for supplying the gyro data in an automotive application. SPI will run at around 1MHz. Can we interface directly through SPI, or should we integrate th...
puis-je utiliser le progiciel X-CUBE-GNSS1 et la carte d'extension X-NUCLEO-IKS01A2 avec une carte Nucleo STM32 pour développer une application combinant à la fois les fonctionnalités GNSS et les capteurs MEMS ? Si oui, comment puis-je les connecter ...
LSM6DSO occasionally indicates Accelerometer data is ready and Gyroscope data is not. But, the odd thing is, if the Gyroscope data is read regardless of it's state of readiness, the Gyroscope values continue to change as expected. Specifically, the...
I would like to find out the if the following assumptions are correct. It offers 16 bit (65K) level resolution. The sensitivity in mV/g would about 3000/2g for the 2g range? That seems rather high because typically you see 500 mv/g values. Also I am ...
I am running a STWINBX1 with the latest v1.2.0 firm from the STM32CubeFunctionPack_DATALOG2_V1.2.0.I have compiled and uploaded the DATALOG2-STWIN.Box firmware successfully. I am using the ST BLE Sensor App v5.0.0 on my iPhone to configure and run t...
Hello,There are some abbreviations next to ODR: HP, HA, LP1, LP2, LP3, and NM. I believe HP stands for high performance, LP stands for low performance, and NM stands for normal mode. Can you explain the differences between LP1, LP2, and LP3? Addition...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.