2022-03-24 11:37 AM
Hi all,
As part of my PhD thesis, I've developed ML algorithms for detecting certain events/phenotypes on cows/cattles using Sensortile.box. However, we are interested in replacing BLE with LoRa. Moreover, we have a custom designed sensor that we want to put on the PCB. However, I'm not able to find the reference PCB design on the website.
I don't see them under 'CAD Resources'. Is this intended?
Thanks,
Yigit Tuncel, PhD Student, ECE
University of Wisconsin-Madison
2022-03-24 1:37 PM
Welcome, @yttuncel, to the community!
Well, the tab CAD Resources contains the GERBER data, the circuit diagram and the parts list. Do you need more information?
Regards
/Peter
2022-03-24 2:30 PM
Hi Peter,
Thanks for the answer!
I'm actually looking for the schematic and layout files which can be opened in Altium Designer (or any other PCB Design Software).
Some of the other design kits in the STM portfolio have the .schdoc/.pcbdoc files in their `CAD Resources` tab. I'm wondering if I can get those for the Sensortile.box.
Best,
Yigit
2022-03-25 12:56 AM
The boards are intended for evaluation and not to be copied (see Terms of Use). Therefore, normally only the GERBER data is published, in order to be able to investigate problems or questions in the layout, furthermore, one can orientate oneself for one's own layout. In this respect, Altium files are not the rule, but the exception.
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.