cancel
Showing results for 
Search instead for 
Did you mean: 

AppsNote for STM32CubeFunctionPack_MOTENV1

Dilbert K
Senior
Posted on July 13, 2017 at 23:03

I just downloaded the new STM32CubeFunctionPack_MOTENV1_V3.0.0 and going through what motion sensor library could do all at once.

As I walk through the code in MEMSCallback(), all the W2ST_CHECK_HW_FEATURE checking is using 'if' and not 'else if'..... So is that meant all features can be detected all at once ?

For instance, can W2ST_HWF_FREE_FALL and W2ST_HWF_PEDOMETER  be enabled at the same time ?? and get correct status ?

Most specific to page 20 on 'en.FP-SNS-MOTENV1_quick_start_guide', it shows all individual Motion features.

However, Mobile Apps would only able to show status one at a time.  Does, features actually running in parallel at firmware background ?

Any doc list out how Application was implemented ?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.