2018-01-31 10:51 AM
Hi.
I am using the X-NUCLEO-IDB04A1 with Nucleo STM32F103 and the available demos are only for F4, L0 and L4. This is fine as I want to learn about programming bluetooth anyway. The BLUENRG chip on the expansion board is also a MCU and can be programmed.
My question is: Do I need to program both devices and if so how, or can I treat the BLUENRG as a simple peripheral and control with standard SPI? Does the BLUENRG need to be programmed or is that only when using it as an MCU?
Thanks.
M.
#nucleo-stm #bluenrg #stm2018-01-31 10:20 PM
Schematic:
Quick guide - it's SPI device:
2018-02-12 9:05 AM
I know that its SPI but looking at the datasheet it actually is more of a complete MCU. As I will already be using an MCU, I dont need two. So I suppose my question is: Can the BLUENRG behave like a simple SPI device, does it need to be flashed seperately, is there default code in it/bootloader, can I read data from SPI straight away. Just looking to know this before I get stuck in.
Thanks.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.