Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to release an IP address

Posted on February 19, 2018 at 17:13Hello,I use a SPWF04SC, and I create a web page on it 's memory.I want to limit the access at only one client.I use the command  'ip_num_clients = 1', that  work good but when the client is dissociated , no more c...

Resolved! SPWF04Sx - AT-S.Http Client Error:1

Posted on January 16, 2018 at 18:30Hi,SPWF04Sx with FW1.1.0, mode miniAPi loaded certificat in the wifi moduleCA, cert and key based on ECC (prime256v1 aka NIST P-256)and i run cmd AT+S.HTTPGET.I have error:+WIND:29:DHCP Reply:192.168.0.2:02:A9:D2:A...

SPWF04Sx - AT+S.HTTPGET - AT-S.Skip CA

Posted on February 12, 2018 at 09:51hi,using AT command AT+S.HTTPGET with option TLS,what does the answer 'AT-S.Skip CA' mean?AT-S.Skip CAAT-S.Skip CAAT-S.Loading:1:2AT-S.Loading:2:2AT-S.Loading:3:2AT-S.Http Server Status Code:200AT-S.OKThanksYoann

aci_gatt_write_char_value return 0x01

Posted on February 01, 2018 at 15:35Hi,I have a bluenrg-1 as a central and a smartphone as a peripheral. Central can connect and discovery correctly.When I try to write a pheriperal's value, aci_gatt_write_char_value() return 0x01.aci_att_prepare_wr...

X-NUCLEO-IDB04A1 with Nucleo STM32F103

Posted on January 31, 2018 at 19:51Hi.I am using the  X-NUCLEO-IDB04A1 with Nucleo STM32F103 and the available demos are only for F4, L0 and L4. This is fine as I want to learn about programming bluetooth anyway. The BLUENRG chip on the expansion bo...

M Greally by Associate II
  • 1561 Views
  • 2 replies
  • 0 kudos

SPBTLE-1S Program

Posted on October 19, 2017 at 04:29Hello, Mr, Ms. I want to program SPBTLE-1S.I want to use the bluetooth module to send signal from MCU to Smartphone. To do that, do I need to program the SPBTLE-1S?How can I do that?I can not find any evaluation bo...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.