2017-04-11 3:12 AM
Hi All,
I need some suggestion regarding my project.
I want my device to send data in wifi direct mode to the Android device which has 3g/4g connectivity.The Android device will then forward the data to the server , so that live tracking happens.
Can Anybody tell how to proceed with this
Kind Regards
Don David
#android #wifi-direct2017-04-11 9:56 AM
Hi David,
ST SPWF0xS modules are not implementing WiFi Direct mode. You can setup the ad-hoc mode, called IBSS into datasheet and user manuals. Or, better, use the miniAP capability. You can setupSPWF module to act as a basic AP, providing link up to 5 devices. Also DHCP/DNS servers are running in this case!
Please refer to this discussion:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.